AXIS#.IL.IUFB
Description
This parameter displays the measured current in the u-winding of the motor for the associated axis.
Versions
Action | Version | Notes |
---|---|---|
Implemented | 02-00-00-000 |
General Information
Type |
Read Only |
Units |
A |
Default Value |
N/A |
Data Type |
Float |
See Also |
N/A |
Stored in Non-Volatile Memory |
No |
Variants Supported
All variants are supported.
Related Topics