DIO#.TERM
Description
Sets whether the bi-directional I/O is terminated or not.
| Value | Description |
|---|---|
| 0 | Not terminated |
| 1 | Terminated |
| 2 | Override feedback auto-termination to not terminated |
| 3 | Override feedback auto-termination to be terminated |
The following table shows what type of termination each bi-directional line supports.
| DIO# | Valid DIO#.TERM Values | Description |
|---|---|---|
| DIO1 to DIO4 | 0 to 3 |
Controls 112Ω termination.
|
| DIO5 | DIO5 is not terminated by default. On newer AKD2G models, DC 136Ω termination is also available. | |
| DIO6 | DIO6 is not terminated. Internal termination is not available. |
Examples
Using DIO# with a differential point-to-point connection:
If the AKD2G is the transmitter DIO#.TERM should be set to 0.
If the AKD2G is the receiver DIO#.TERM should be set to 1.
Using DIO# with differential multi-drop connection:
If the AKD2G is the transmitter DIO#.TERM should be set to 0.
If the AKD2G is the receiver the DIO#.TERM should be set to 1 on the last drive. The other receivers should have DIO#.TERM set to 0.
Connecting a single-ended, open-collector device to a DIO input.
The DIO#.TERM should be set to 0. The negative pin should be left disconnected / floating. Internal resistors in the drive will pull this to an appropriate level. The open-collector device should be connected between the positive pin and GND_I/O. The diagram below shows the bias resistors that are inside the drive.
Context
For more information see Digital Inputs and Outputs.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
| Type | Read/Write |
| Units | N/A |
| Range | 0 to 1 |
| Default Value | 0 |
| Data Type | Integer |
| See Also | |
|
Stored in Non-Volatile Memory |
Yes |
Variants Supported
All variants are supported.
Fieldbus Information
|
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
PDO Mappable |
|---|---|---|---|---|---|---|---|
|
DIO1.TERM |
368ah |
07h |
Unsigned8 |
- |
- |
Read/Write |
No |
|
DIO2.TERM |
368bh |
07h |
Unsigned8 |
- |
- |
Read/Write |
No |
|
DIO3.TERM |
368ch |
07h |
Unsigned8 |
- |
- |
Read/Write |
No |
|
DIO4.TERM |
368dh |
07h |
Unsigned8 |
- |
- |
Read/Write |
No |
|
DIO5.TERM |
368eh |
07h |
Unsigned8 |
- |
- |
Read/Write |
No |
|
DIO6.TERM |
368fh |
07h |
Unsigned8 |
- |
- |
Read/Write |
No |
|
ID |
Instance |
Attribute |
Name |
Data Type |
Access |
User Mappable |
|---|---|---|---|---|---|---|
|
22350 |
1 |
22350 (0x574e) |
DIO1.TERM |
Unsigned8 |
Read/Write |
Yes |
|
22351 |
1 |
22351 (0x574f) |
DIO2.TERM |
Unsigned8 |
Read/Write |
Yes |
|
22352 |
1 |
22352 (0x5750) |
DIO3.TERM |
Unsigned8 |
Read/Write |
Yes |
|
22353 |
1 |
22353 (0x5751) |
DIO4.TERM |
Unsigned8 |
Read/Write |
Yes |
|
22354 |
1 |
22354 (0x5752) |
DIO5.TERM |
Unsigned8 |
Read/Write |
Yes |
|
22355 |
1 |
22355 (0x5753) |
DIO6.TERM |
Unsigned8 |
Read/Write |
Yes |
|
Parameter |
PNU |
Data Type |
Access |
Units |
|---|---|---|---|---|
|
DIO1.TERM |
22350 |
Unsigned8 |
Read/Write |
- |
|
DIO2.TERM |
22351 |
Unsigned8 |
Read/Write |
- |
|
DIO3.TERM |
22352 |
Unsigned8 |
Read/Write |
- |
|
DIO4.TERM |
22353 |
Unsigned8 |
Read/Write |
- |
|
DIO5.TERM |
22354 |
Unsigned8 |
Read/Write |
- |
|
DIO6.TERM |
22355 |
Unsigned8 |
Read/Write |
- |