DOUT#.SOURCEID
Description
DOUT#.SOURCEID sets the digital output source ID, for sources that require an ID.
Examples
Usage
DOUT#.SOURCEID can be used to select the compare channel when DOUT#.SOURCE = 4 (Compare).
Code
The following commands set the source of digital output 2 to compare channel 1, and digital output 3 to compare channel 2.
--> DOUT2.SOURCE 4
--> DOUT2.SOURCEID 1
--> DOUT3.SOURCE 4
--> DOUT3.SOURCEID 2
Context
For more information see Digital Inputs and Outputs.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 | |
| Added Compare channel support | 02-06-00-000 |
General Information
| Type | Read/Write |
| Units | N/A |
| Range | 1 to 2 |
| Default Value | 0 |
| Data Type | Integer |
| See Also | N/A |
|
Stored in Non-Volatile Memory |
Yes |
Variants Supported
All variants are supported
Fieldbus Information
|
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
PDO Mappable |
|---|---|---|---|---|---|---|---|
|
DOUT1.SOURCEID |
360ah |
02h |
Unsigned8 |
- |
- |
Read/Write |
No |
|
DOUT2.SOURCEID |
360bh |
02h |
Unsigned8 |
- |
- |
Read/Write |
No |
|
DOUT3.SOURCEID |
360ch |
02h |
Unsigned8 |
- |
- |
Read/Write |
No |
|
DOUT4.SOURCEID |
360dh |
02h |
Unsigned8 |
- |
- |
Read/Write |
No |
|
DOUT5.SOURCEID |
360eh |
02h |
Unsigned8 |
- |
- |
Read/Write |
No |
|
DOUT6.SOURCEID |
360fh |
02h |
Unsigned8 |
- |
- |
Read/Write |
No |
|
DOUT7.SOURCEID |
3610h |
02h |
Unsigned8 |
- |
- |
Read/Write |
No |
|
DOUT8.SOURCEID |
3611h |
02h |
Unsigned8 |
- |
- |
Read/Write |
No |
|
DOUT9.SOURCEID |
3612h |
02h |
Unsigned8 |
- |
- |
Read/Write |
No |
|
ID |
Instance |
Attribute |
Name |
Data Type |
Access |
User Mappable |
|---|---|---|---|---|---|---|
|
21200 |
1 |
21200 (0x52d0) |
DOUT1.SOURCEID |
Unsigned8 |
Read/Write |
Yes |
|
21201 |
1 |
21201 (0x52d1) |
DOUT2.SOURCEID |
Unsigned8 |
Read/Write |
Yes |
|
21202 |
1 |
21202 (0x52d2) |
DOUT3.SOURCEID |
Unsigned8 |
Read/Write |
Yes |
|
21203 |
1 |
21203 (0x52d3) |
DOUT4.SOURCEID |
Unsigned8 |
Read/Write |
Yes |
|
21204 |
1 |
21204 (0x52d4) |
DOUT5.SOURCEID |
Unsigned8 |
Read/Write |
Yes |
|
21205 |
1 |
21205 (0x52d5) |
DOUT6.SOURCEID |
Unsigned8 |
Read/Write |
Yes |
|
21206 |
1 |
21206 (0x52d6) |
DOUT7.SOURCEID |
Unsigned8 |
Read/Write |
Yes |
|
21207 |
1 |
21207 (0x52d7) |
DOUT8.SOURCEID |
Unsigned8 |
Read/Write |
Yes |
|
21208 |
1 |
21208 (0x52d8) |
DOUT9.SOURCEID |
Unsigned8 |
Read/Write |
Yes |
|
Parameter |
PNU |
Data Type |
Access |
Units |
|---|---|---|---|---|
|
DOUT1.SOURCEID |
21200 |
Unsigned8 |
Read/Write |
- |
|
DOUT2.SOURCEID |
21201 |
Unsigned8 |
Read/Write |
- |
|
DOUT3.SOURCEID |
21202 |
Unsigned8 |
Read/Write |
- |
|
DOUT4.SOURCEID |
21203 |
Unsigned8 |
Read/Write |
- |
|
DOUT5.SOURCEID |
21204 |
Unsigned8 |
Read/Write |
- |
|
DOUT6.SOURCEID |
21205 |
Unsigned8 |
Read/Write |
- |
|
DOUT7.SOURCEID |
21206 |
Unsigned8 |
Read/Write |
- |
|
DOUT8.SOURCEID |
21207 |
Unsigned8 |
Read/Write |
- |
|
DOUT9.SOURCEID |
21208 |
Unsigned8 |
Read/Write |
- |