DOUT#.STATE
Description
Reads the state of one digital output according to the number identified in the command.
Examples
Code
--> DOUT1.STATE 1
Context
For more information see Digital Inputs and Outputs.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
| Type | Read Only |
| Units | N/A |
| Range | 0 to 1 |
| Default Value | N/A |
| Data Type | Integer |
| See Also | |
|
Stored in Non-Volatile Memory |
No |
Variants Supported
All variants are supported.
Fieldbus Information
|
ID |
Instance |
Attribute |
Name |
Data Type |
Access |
User Mappable |
|---|---|---|---|---|---|---|
|
21000 |
1 |
21000 (0x5208) |
DOUT1.STATE |
Unsigned8 |
Read Only |
Yes |
|
21001 |
1 |
21001 (0x5209) |
DOUT2.STATE |
Unsigned8 |
Read Only |
Yes |
|
21002 |
1 |
21002 (0x520a) |
DOUT3.STATE |
Unsigned8 |
Read Only |
Yes |
|
21003 |
1 |
21003 (0x520b) |
DOUT4.STATE |
Unsigned8 |
Read Only |
Yes |
|
21004 |
1 |
21004 (0x520c) |
DOUT5.STATE |
Unsigned8 |
Read Only |
Yes |
|
21005 |
1 |
21005 (0x520d) |
DOUT6.STATE |
Unsigned8 |
Read Only |
Yes |
|
21006 |
1 |
21006 (0x520e) |
DOUT7.STATE |
Unsigned8 |
Read Only |
Yes |
|
21007 |
1 |
21007 (0x520f) |
DOUT8.STATE |
Unsigned8 |
Read Only |
Yes |
|
21008 |
1 |
21008 (0x5210) |
DOUT9.STATE |
Unsigned8 |
Read Only |
Yes |
|
Parameter |
PNU |
Data Type |
Access |
Units |
|---|---|---|---|---|
|
DOUT1.STATE |
21000 |
Unsigned8 |
Read Only |
- |
|
DOUT2.STATE |
21001 |
Unsigned8 |
Read Only |
- |
|
DOUT3.STATE |
21002 |
Unsigned8 |
Read Only |
- |
|
DOUT4.STATE |
21003 |
Unsigned8 |
Read Only |
- |
|
DOUT5.STATE |
21004 |
Unsigned8 |
Read Only |
- |
|
DOUT6.STATE |
21005 |
Unsigned8 |
Read Only |
- |
|
DOUT7.STATE |
21006 |
Unsigned8 |
Read Only |
- |
|
DOUT8.STATE |
21007 |
Unsigned8 |
Read Only |
- |
|
DOUT9.STATE |
21008 |
Unsigned8 |
Read Only |
- |