DRV.CLRFAULTS

Description

DRV.CLRFAULTS tries to clear all active faults and warnings on all the axis.

When a fault occurs on an axis, the fault is set and can only be cleared by:

If the DRV.CLRFAULTS succeeds, then AXIS#.FAULTS on all the axes indicate no faults exist. If the fault still exists on an axis after DRV.CLRFAULTS, the fault remains on that axis.

See Faults and Warning Messages for details regarding the behavior of individual faults.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Command

Units

N/A

Range

N/A

Default Value

N/A

Data Type

N/A

Stored in Non-Volatile Memory

No

Variants Supported

All variants are supported.

Fieldbus Information

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

DRV.CLRFAULTS

2002

7D2

Unsigned8

Read/Write

-

PROFINET

Parameter

PNU

Data Type

Access

Units

DRV.CLRFAULTS

2002

Unsigned8

Read/Write

-

Related Topics

AXIS#.FAULTS, AXIS#.EN , AXIS#.DIS ,AXIS#.CLRWARNINGS