FB#.PRINTMOTORDATA

Description

FB#.PRINTMOTORDATA reads the contents of the motor data file stored in feedback memory if the feedback device supports motor memory.

Context

See Feedback # View.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read Only

Units

N/A

Range

N/A

Default Value

N/A

Data Type

String

Stored in Non-Volatile Memory

No

Variants Supported

All variants are supported.