FB#.SIGNALSIN
Description
This parameter returns the measured analog sine channel signal of a connected resolver or sine/cosine encoder.
This parameter is only available on the following encoder types:
- Sine Encoder with Halls
- Sine Encoder without Halls
- EnDat Analog
- Resolver
- HIPERFACE
- BiSS-B with SinCos
These commands are not recordable on FB1 and FB2.
For recording on FB1 and FB2, see FB#.MONITOR#.SOURCE and FB#.MONITOR#.DATA.
Examples
Usage
The sine signal measurement can be used to detect if a sine/cosine encoder was commissioned correctly.
Code
--> FB3.SIGNALSIN
0.423 [V]
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-02-000 |
General Information
|
Type |
Read Only |
|
Units |
V |
|
Range |
N/A |
|
Default Value |
N/A |
|
Data Type |
Float |
| Stored in Non-Volatile Memory | No |
Variants Supported
All variants are supported.
Fieldbus Information
|
ID |
Instance |
Attribute |
Name |
Data Type |
Access |
User Mappable |
|---|---|---|---|---|---|---|
|
30300 |
1 |
30300 (0x765c) |
FB1.SIGNALSIN |
Signed32 |
Read Only |
Yes |
|
30301 |
1 |
30301 (0x765d) |
FB2.SIGNALSIN |
Signed32 |
Read Only |
Yes |
|
30302 |
1 |
30302 (0x765e) |
FB3.SIGNALSIN |
Signed32 |
Read Only |
Yes |
|
30303 |
1 |
30303 (0x765f) |
FB4.SIGNALSIN |
Signed32 |
Read Only |
Yes |
|
30304 |
1 |
30304 (0x7660) |
FB5.SIGNALSIN |
Signed32 |
Read Only |
Yes |
|
Parameter |
PNU |
Data Type |
Access |
Units |
|---|---|---|---|---|
|
FB1.SIGNALSIN |
30300 |
Float |
Read Only |
- |
|
FB2.SIGNALSIN |
30301 |
Float |
Read Only |
- |
|
FB3.SIGNALSIN |
30302 |
Float |
Read Only |
- |
|
FB4.SIGNALSIN |
30303 |
Float |
Read Only |
- |
|
FB5.SIGNALSIN |
30304 |
Float |
Read Only |
- |
Related Topics