VBUS.OVWTHRESH
Description
This parameter is the DC bus overvoltage warning threshold. When the measured DC bus voltage exceeds the threshold, an overvoltage warning is thrown.
Examples
Usage
The default value of VBUS.OVWTHRESH is 0, which turns the overvoltage warning off.
If this parameter is nonzero, the drive throws Warning 2006: Bus over voltage, when the measured DC bus voltage VBUS.VALUE is greater than VBUS.OVWTHRESH. It clears the warning when VBUS.VALUE drops below 97% of VBUS.OVWTHRESH.
Code
When VBUS.OVWTHRESH is set to 0, the drive does not report an overvoltage warning.
--> VBUS.OVWTHRESH 0 [Vdc] --> VBUS.VALUE 403.723 [Vdc] --> DRV.WARNINGS No warnings active
Change the overvoltage warning level to a nonzero value. When the bus voltage is higher than this value, the overvoltage warning is reported on each axis.
--> VBUS.OVWTHRESH 400 --> VBUS.OVWTHRESH 400 [Vdc] --> VBUS.VALUE 403.723 [Vdc] --> DRV.WARNINGS 1-2006: Warning: Bus over voltage. 2-2006: Warning: Bus over voltage.
When the bus voltage drops below the VBUS.OVWTHRESH, but is still greater than 97% of the threshold, the warning persists.
--> VBUS.VALUE 394.272 --> DRV.WARNINGS 1-2006: Warning: Bus over voltage. 2-2006: Warning: Bus over voltage.
When the bus voltage drops below 97% of VBUS.OVWTHRESH, the warning is removed.
--> VBUS.VALUE 378.521 --> DRV.WARNINGS No warnings active
Context
For more information on DC bus protection, see Power and Regeneration.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
| Type | Read/Write |
| Units | Vdc |
| Range | 0 to 900 |
| Default Value | 0 (warning disabled) |
| Data Type | Integer |
| See Also | VBUS.VALUE, VBUS.OVFTHRESH |
|
Stored in Non-Volatile Memory |
Yes |
Variants Supported
All variants are supported.
Fieldbus Information
|
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
PDO Mappable |
|---|---|---|---|---|---|---|---|
|
VBUS.OVWTHRESH |
300ah |
08h |
Unsigned16 |
- |
- |
Read/Write |
No |
|
ID |
Instance |
Attribute |
Name |
Data Type |
Access |
User Mappable |
|---|---|---|---|---|---|---|
|
2508 |
1 |
2508 (0x9cc) |
VBUS.OVWTHRESH |
Unsigned16 |
Read/Write |
Yes |
|
Parameter |
PNU |
Data Type |
Access |
Units |
|---|---|---|---|---|
|
VBUS.OVWTHRESH |
2508 |
Unsigned16 |
Read/Write |
- |