Scaled Feedback
For feedback not associated with an axis, a set of scaled feedback parameters are provided to optionally represent the feedback position in scaled units.
- FB Monitor PIN (FB#.SCALED.PIN) and FB Monitor POUT (FB#.SCALED.POUT) specify the scaling ratio.
- Direction (FB#.SCALED.DIR) sets the direction of the scaled position.
- Offset (FB#.SCALED.OFFSET) sets an offset adjustment.
- Unit Label (FB#.SCALED.LABEL) is a short units text description.
The Scaled Position is calculated as follows:
| FB#.SCALED.DIR | Direction Sign |
|---|---|
| 0 | 1 |
| 1 | -1 |
Dual-Loop
There are separate feedback sources for the current, velocity, and position loops. By default they’re all set to the current loop feedback source (AXIS#.IL.FBSOURCE). If a separate feedback is desired for the different loops, those sources can be set independently using AXIS#.VL.FBSOURCE and AXIS#.PL.FBSOURCE .
Electronic Gearing
For Electronic Gearing, AXIS#.GEAR.FBSOURCE is also available. See the Electronic Gearing feature for more information.
Jump to a section about Feedback:
- Feedback Views
- Feedback Configuration
- Feedback Methods
- Smart Feedback Adapter (SFA)
- Non-Plug and Play Feedback Devices