AOUT.CUTOFF
Description
AOUT.CUTOFF sets the cutoff frequency in Hz for a single-pole low-pass
filter on the Analog Output.
A value of 0 Hz will turn off the filter and will allow all frequencies to pass through.
The filter can be used with all modes of Analog Output.
General Information
Type |
NV Parameter |
Units |
Hz |
Range |
0 to 10,000 Hz |
Default Value |
0 Hz |
Data Type |
Float |
Start Version |
M_01-04-01 |
Variants Supported
*In SynqNet, a parameter may be available in the firmware but have no effect on the system. See SynqNet Supported Parameters.
Index/Subindex | Object Start Version |
---|---|
3470h/6 |
M_01-04-01-000 |