AOUT.OFFSET
Description
This parameter sets the analog output offset.
General Information
Type |
NV Parameter |
Units |
V |
Range |
-10 to +10 V |
Default Value |
0 V |
Data Type |
Float |
Start Version |
M_01-00-00-000 |
Variants Supported
*In SynqNet, a parameter may be available in the firmware but have no effect on the system. See SynqNet Supported Parameters.
Index/Subindex | Object Start Version |
---|---|
500Bh/0 |
M_01-00-00-000 |