DRV.DBILIMIT

Description

This parameter sets the maximum amplitude of the current for dynamic braking.

Example

Setting DRV.DBILIMIT to 2 limits the dynamic brake current to 2 Arms.

General Information

Type

NV Parameter

Units

Arms

Range

0 to minimum of drive peak current (DRV.IPEAK) and motor peak current (MOTOR.IPEAK).

Default Value

Minimum of drive continuous current (DRV.ICONT) and motor continuous current (MOTOR.ICONT).

Data Type

Float

Start Version

M_01-00-00-000

Variant Supported
MKD EtherCAT Yes
AKD-N Yes
MKD-N Yes
MKD-C No
EtherCAT CoE and CANopen
Index/Subindex Object Start Version

3444h/0

M_01-00-00-000

Related Topics

"Controlled Stop"

CS Parameters

DRV.DISMODE

"Dynamic Braking"