DRV.ICONT
Description
DRV.ICONT returns the drive continuous rated current in Arms.
General Information
|
Type |
R/O Parameter |
|
Units |
Arms |
|
Range |
N/A |
|
Default Value |
N/A |
|
Data Type |
Float |
|
Start Version |
M_01-00-00-000 |
| Variant | Supported |
|---|---|
| MKD EtherCAT | Yes |
| AKD-N | Yes |
| MKD-N | Yes |
| MKD-C | Yes |
| Index/Subindex | Object Start Version |
|---|---|
|
5083h/0 |
M_01-00-00-000 |