ECAT.LEGACYREV

Description

The ECAT.LEGACYREV changes the displayed revision number in the EtherCAT slave information (SII).

Value Description
0 The revision number is changed with every Beta or production firmware, that includes changes in the CANopen-behaviour. With this setting EoE and the third FMMU for mailbox checking is enabled by using the ESI-file. The size of the Rx-PDOs is 32 bytes.
1 Revision number is set to legacy value of #x00000002. With this setting the Rx-PDO size is restricted to 20 bytes.

General Information

Type

NV Parameter

Units

N/A

Range

0 to 1

Default Value

1

Data Type

Integer

Start Version

M_01-16-00-001

EtherCAT CoE and CANopen
Index/Subindex Object Start Version
541Dh/1 M_01-16-00-001