IL.FB

Description

This parameter reads the measured, de-rotated actual current value of the motor.


  • Internally the resolution of the current scale is 20130 increments.
    For an AKD with a peak current of 9 amps, the current resolution applied is 9/20130 = .447 mA.
    For a 48 amp peak current drive, the resolution is 48/20130 = 2.38 mA.
    The current scaling is hard coded and cannot be changed by decreasing the peak current settings in the drive.

General Information

Type

R/O Parameter

Units

Arms

Range

± Drive peak current (DRV.IPEAK)

Default Value

N/A

Data Type

Float

See Also

N/A

Start Version

M_01-00-00-000

Variant Supported
AKD EtherCAT Yes
AKD-N Yes
AKD-N Yes
AKD-C No
EtherCAT CoE and CANopen
Index/Subindex Object Start Version
3558h/0 M_01-00-00-000

Related Topics

"Current Loop"