IL.KP

Description

IL.KP is used to modify the proportional gain of the PI-loop that controls the q-component of the current.

General Information

Type

NV Parameter

Units

V/A

Range

0 to 2,000 V/A

Default Value

Read from the motor or, if no memory, 50.009 V/A

Data Type

Float

See Also

N/A

Start Version

M_01-00-00-000

Variant Supported
MKD EtherCAT Yes
AKD-N Yes
MKD-N Yes
MKD-C No
EtherCAT CoE and CANopen
Index/Subindex Object Start Version
3598h/0 M_01-00-00-000

Related Topics

"Current Loop"