MOTOR.RTYPE

Description

This parameter defines the type of thermal resistor used inside of the motor to measure motor temperature. The following resistor types are supported:

For firmware versions prior to 01-10-02-000, parameter range is 0 to 1.

MOTOR.RTYPE Thermal Resistor Type
0 PTC
1 NTC

For firmware versions 01-10-02-000 and later, parameter range is 0 to 127.

MOTOR.RTYPE Thermal Resistor Type
0 Single PTC
1 Single NTC
2 KTY83-110
3 KTY84-130
4 PTC + KTY83-110
5 Thermal switch
6 PTC + PT1000
7 Dual PTC
8 PT1000
127 No sensor

  • For firmware versions 01-09-00-000 and later, this parameter is automatically configured for Kollmorgen motors when MOTOR.AUTOSET = 1.

General Information

Type

NV Parameter

Units

N/A

Range

0 to 1 for firmware versions before 01-10-02-000

0 to 8, 127 for firmware version 01-10-02-000 and later

Default Value

0

Data Type

Integer

Start Version

M_01-00-00-000

Variant Supported
MKD EtherCAT Yes
AKD-N Yes
MKD-N Yes
MKD-C No
EtherCAT CoE and CANopen
Index/Subindex Object Start Version

50FEh/0

M_01-00-00-000

Related Topics

Motor View