MOTOR.VOLTMIN

Description

This parameter configures the drive for the induction motor's minimum voltage at standstill. It is given as a percentage (%) of the motor’s rated voltage. MOTOR.VOLTMIN is used to calculate the constant volts per Hertz characteristics of the drive and motor and should be set to a value that generates a current of about 40% of the rated current at standstill.

General Information

Type

NV Parameter

Units

%

Range

0 to 100%

Default Value

2%

Data Type

U16

See Also

MOTOR.VRATED, MOTOR.VOLTRATED

Start Version

 

Variant Supported
MKD EtherCAT Yes
AKD-N Yes
MKD-N Yes
MKD-C No
EtherCAT CoE and CANopen
Index/Subindex Object Start Version
3457h/3 M_01-00-00-000

Related Topics

"Motor View"