PL.CMD
Description
PL.CMD reads the position command as it is received in the position loop entry.
General Information
Type |
R/O Parameter |
Units |
Depends on UNIT.PLINEAR (pg 1) or UNIT.PROTARY (pg 1) Rotary: counts, rad, deg, (custom units), 16-bit counts Linear: counts, mm, µm, (custom units), 16-bit counts |
Range |
N/A |
Default Value |
N/A |
Data Type |
Float
|
See Also |
|
Start Version |
M_01-00-00-000 |
Variant | Supported |
---|---|
MKD EtherCAT | Yes |
AKD-N | Yes |
MKD-N | Yes |
MKD-C | No |
Related Topics