PL.KI
Description
PL.KI sets the integral gain of the position regulator PID loop.
General Information
Type |
NV Parameter |
Units |
Hz |
Range |
0 to 250 Hz |
Default Value |
0 Hz |
Data Type |
Float |
See Also |
PL.KP, PL.KD |
Start Version |
M_01-00-00-000 |
Variant | Supported |
---|---|
MKD EtherCAT | Yes |
AKD-N | Yes |
MKD-N | Yes |
MKD-C | No |
Index/Subindex | Object Start Version |
---|---|
3480h/0 | M_01-00-00-000 |
Related Topics