VBUS.VALUE

Description

VBUS.VALUE reads the DC bus voltage.

General Information

Type

R/O Parameter

Units

VDC

Range

0 to 900VDC

Default Value

N/A

Data Type

Float

See Also

N/A

Start Version

M_01-00-00-000

Variant Supported
MKD EtherCAT Yes
AKD-N Yes
MKD-N Yes
MKD-C Yes

EtherCAT CoE and CANopen

Index/Subindex Object Start Version
361Ah/0 M_01-00-00-000

Related Topics

1   Regeneration