Insert FBD Objects on a Line
- This feature is available for all objects having one input pin and one output pin (e.g., variable boxes, contacts, coils).
- This feature is mainly useful when entering elements of Ladder Diagrams.
- Draw a horizontal line between left and right power rails: it is the rung.
- Then insert contacts and coils on the line to build the FFLD rung.