FBD Network Breaks
Network breaks can be entered anywhere in an FBD diagram.
- Breaks have no meaning for the execution of the program; they just help in understanding big diagrams, by splitting them into a list of networks.
- Select the Insert Network Break button in the FBD toolbar to insert a new break:
![]()
Insert network break: In this mode, the mouse is used for inserting a horizontal line that acts as a break in the diagram.
- The break line is drawn on the whole diagram width.
- No other object can overlap a network break.
- Break lines can then be selected and moved vertically to another location.
- Network breaks can also be used to browse the diagram.
- Press the Ctrl+Page Up or Ctrl+Page Down keys to move the selection to the next or previous network break.