FBD OR Vertical Rail
The FBD Editor enables the drawing of FFLD rungs.
- The OR rail can be inserted on a rung in order to connect parallel contacts together.
- In the FBD toolbar , click the Insert OR Rail button (
) to insert a new OR rail. - In this mode, the mouse is used to insert a rail that collects several Boolean data flows for an OR operation to insert parallel contacts (e.g., Ladder Diagrams).
- The OR rail has exactly the same meaning as an OR block regarding the execution of the diagram.