Using the FBD Toolbar
Click the applicable button before using the mouse in the graphic area.
|
Tool |
Button |
Description |
|---|---|---|
|
Execution Order |
|
Show the execution order of the elements in the diagram. |
|
Insert "OR" Rail |
|
In this mode, the mouse is used to insert a rail that collects several Boolean data flows for an OR operation. This is used to insert parallel contacts, as in Ladder Diagrams. |
|
Insert Block |
|
In this mode, the mouse is used for inserting blocks in the diagram.
|
|
Insert Coil |
|
In this mode, the mouse is used to insert a coil in the diagram (e.g., Ladder Diagrams). It is not required that a coil be connected on its right side. |
|
Insert Comment Text |
|
In this mode, the mouse is used for inserting comment text areas in the diagram.
|
|
Insert Connection Line |
|
In this mode, the mouse is used to wire the input and output pins of the diagram objects.
|
|
Insert Contact |
|
In this mode, the mouse is used to insert a contact in the diagram (e.g., Ladder Diagrams). |
|
|
In this mode, the mouse is used for inserting a user-defined corner on a line.
|
|
|
|
In this mode, the mouse is used to insert jump symbols in the diagram.
|
|
|
Insert Label |
|
In this mode, the mouse is used for inserting a label in the diagram.
|
|
Insert Left Power Rail |
|
In this mode, the mouse is used to insert a left power rail in the diagram.
|
|
Insert Network Break |
|
In this mode, the mouse is used for inserting a horizontal line that acts as a break in the diagram.
|
|
Insert Right Power Rail |
|
In this mode, the mouse is used to insert a right power rail in the diagram.
|
|
Insert Variable |
|
In this mode, the mouse is used for inserting variable tags.
|
|
Selection |
|
In this mode, you cannot insert any elements into the diagram.
|
|
Swap Item Style |
|
Change the text justification. |