Bookmarks
- Insert bookmarks anywhere in a document.
- Use them to jump from one bookmark to another with a single command for browsing the document.
- Bookmarks are supported in all program editors plus the Variable editor.
These are the available commands for using bookmarks:
|
Command |
Description |
|---|---|
|
Ctrl + F2 |
Toggle the bookmark at the current position. |
|
Shift + F2 |
Go to the next bookmark. |
According to the type of document, the possible locations for a bookmark are:
- In the FBD editor, a bookmark is placed on any FBD object (not on a line).
- In the FFLD editor, a bookmark is placed on a rung header.
- In the SFC editor, a bookmark is placed on an SFC symbol (step, transition, jump...).
- In the text editor, a bookmark is placed on a line of text.
- In the Variable editor, a bookmark is placed on any line of the grid (variable or group).
-
-
Bookmarks are valid only while the editing window is open.
They are not stored in the document when the window is closed.