MC_GrpWriteParam

PLCopen motion icon Pipe Network motion icon

 Function Block - Writes a value to the specified group parameter.

Inputs

Input

Data Type

Range

Unit

Default

Description

Execute

BOOL

FALSE, TRUE

N/A

No default

On the rising edge, request to write a value to the specified Boolean group parameter.

AxesGroupRef

AXES_GROUP_REF

No range

N/A

No default

The axis group the Boolean parameter value is written to.

ParamNum

LREAL

See Axes Group Parameters.

LREAL

No default

Only one parameter is supported:
MC_GRP_PARAM_CIRCLE_TOLERANCE:

ParamValue

UINT

Parameter dependent.

Parameter dependent.

No default

The new value for the group parameter.

Outputs

Output

Data Type

Range

Unit

Description

Done

BOOL

FALSE, TRUE

N/A

If TRUE, the command completed successfully.

Busy

BOOL

FALSE, TRUE

N/A

If TRUE, the function block is executing.

Error

BOOL

FALSE, TRUE

N/A

If TRUE, an error has occurred.

ErrorID

INT

Enumerated

N/A

Remarks

Figure 1: MC_GrpWriteParam

FBD Language Example

FFLD Language Example

IL Language Example

Not available.

ST Language Example

Inst_MC_GrpWriteParam( DoExecute, Group1_ref, MC_GRP_PARAM_CIRCLE_TOLERANCE, CircleTolerance );

See Also