MC_ReadStatus
Function Block - Returns the state of the specified axis.
Inputs
|
Input |
Data Type |
Range |
Unit |
Default |
Description |
|---|---|---|---|---|---|
|
Enable |
BOOL |
FALSE, TRUE |
N/A |
No default |
Request to read and return the axis status. |
|
Axis |
AXIS_REF |
1 to 256 |
N/A |
No default |
Name of a declared instance of the AXIS_REF library function.
|
Outputs
|
Output |
Data Type |
Range |
Unit |
Description |
|---|---|---|---|---|
|
Valid |
BOOL |
FALSE, TRUE |
N/A |
Indicates the outputs are valid. |
|
Busy |
BOOL |
FALSE, TRUE |
N/A |
Indicates this function block is executing. |
|
Error |
BOOL |
FALSE, TRUE |
N/A |
Indicates an invalid input was specified. |
|
ErrorID |
INT |
-32768 to +32767 |
|
Indicates the error if Error output is TRUE. |
|
ErrorStop |
BOOL |
FALSE, TRUE |
N/A |
Indicates Error Stop state. Either E-stop or C-stop. |
|
Disabled |
BOOL |
FALSE, TRUE |
N/A |
Indicates Disabled state. Open loop and drive is disabled. |
|
Stopping |
BOOL |
FALSE, TRUE |
N/A |
Indicates Stopping state. MC_Stop command. |
|
StandStill |
BOOL |
FALSE, TRUE |
N/A |
Indicates Stand Still state. No move, closed loop, drive enabled. |
|
DiscreteMotion |
BOOL |
FALSE, TRUE |
N/A |
Indicates Discrete Motion state. Pprogrammed endpoint move is active. |
|
ContinuousMotion |
BOOL |
FALSE, TRUE |
N/A |
Indicates Continuous Motion state. Unending, single-axis move is active. |
|
SynchronizedMotion |
BOOL |
FALSE, TRUE |
N/A |
Indicates Synchronized Motion state Slave move is active. |
|
Homing |
BOOL |
FALSE, TRUE |
N/A |
Indicates Homing state. A homing cycle is currently executing. |
|
ConstantVelocity |
BOOL |
FALSE, TRUE |
N/A |
Indicates the axis is moving at a constant velocity. |
|
Accelerating |
BOOL |
FALSE, TRUE |
N/A |
Indicates the axis is accelerating. |
|
Decelerating |
BOOL |
FALSE, TRUE |
N/A |
Indicates the axis is decelerating. |
Remarks
-
-
This function or function block returns cached data.
See Program a Multi-Core Controller.
See Function Blocks - General Rules about how inputs and outputs work.
Figure 1: MC_ReadStatus
FBD Language Example
Not available.
FFLD Language Example
IL Language Example
Not available.
ST Language Example
(* MC_ReadStatus ST example *)
Inst_MC_ReadStatus( EnableRead, Axis1 );
//Inst_MC_ReadStatus is an instance of MC_ReadStatus function block
AxisStopping := Inst_MC_ReadStatus.Stopping; // store Stopping output to a user defined variable
AxisAccelerating := Inst_MC_ReadStatus.Accelerating; // store Accelerating output to a user defined variable