MLAxisReadFEUU

Pipe Network motion icon

 Function - Returns the difference between the reference position and the actual position of the drive mapped to the specified axis.

Inputs

Input

Data Type

Range

Unit

Default

Description

ID

DINT

1 to 1024

N/A

No default

Pipe network identifier of the axis block.

Outputs

Output

Data Type

Range

Unit

Description

Error

LREAL

 

User units

Returns the difference between the reference position and the actual position of the drive mapped to the specified axis.

Remarks

None

FBD Language Example

FFLD Language Example

IL Language Example

Not available.

ST Language Example

Axis1_Error := MLAxisReadFEUU(PipeNetwork.Axis1 )  ;

See Also

MLAxisReadActPos