MLAxisReadActPos

Pipe Network motion icon

 Function - Returns the actual position of the axis.

Inputs

Input

Data Type

Range

Unit

Default

Description

ID

DINT

1 to 1024

N/A

No default

ID of the Axis block.

Outputs

Output

Data Type

Range

Unit

Description

Default (.Q)

BOOL

FALSE, TRUE

N/A

Position

LREAL

 

User units

Remarks

  • Previous function name: MLAxisActualPos

FBD Language Example

FFLD Language Example

IL Language Example

Not available.

ST Language Example

Axis1_Position := MLAxisReadActPos( PipeNetwork.Axis1 ) ;

See Also