MLAxisWritePipPos

Pipe Network motion icon

 Function - Forces the pipe position internal value.

  • Changes the pipe position to be the new value.
  • May cause a jump in motion.

  • This function works only when no pipe is connected.

Input

Data Type

Range

Unit

Default

Description

AxisID

DINT

1 to 1024

N/A

No default

ID of the Axis block.

PipePosition

LREAL

No range

User units

No default

Sets the Axis Pipe Position.

See Set the Axis Block Position Units.

Outputs

Output

Data Type

Range

Unit

Description

Default (.Q)

BOOL

FALSE, TRUE

N/A

Remarks

None

FBD Language Example

FFLD Language Example

IL Language Example

Not available.

ST Language Example

 
MLAxisWritePipPos(PipeNetwork.Axis1, 3000 ) ;

See Also