MLCamInit
Function - Initializes a CAM Pipe Block for use in a PLC Program.
Inputs
|
Input |
Data Type |
Range |
Unit |
Default |
Description |
|---|---|---|---|---|---|
|
BlockID |
DINT |
1 to 1024 |
N/A |
No default |
ID number of a created Pipe Block. |
|
ProfileName |
STRING |
No range |
N/A |
No default |
|
|
ModuloPosition |
LREAL |
0 to 1.0x10300 |
User units |
No default |
|
Outputs
|
Output |
Data Type |
Range |
Unit |
Description |
|---|---|---|---|---|
|
Default (.Q) |
BOOL |
FALSE, TRUE |
N/A |
|
Remarks
This function is automatically called if a CAM Block is added to the Pipe Network, with user-defined settings then entered in the Pipe Blocks Properties screen.
- The CAM Pipe Block is used to generate motion profiles of any shape.
- These profiles are created and initiated separately and the shape is modified with the CAM Editor.
- With the Editor profiles can be changed graphically or by manually changing values in a numeric table relating input and output values with specific slopes.
- The CAM Editor software tool provides the capability to visualize, analyze, edit, and smooth profiles.
With the Pipe Network (PN) CAM block:
- The CAM block’s profile is in reference to the input positions coming into the PN CAM block (Master Absolute)
- The PN CAM block output positions are in reference to PN CAM block’s output position at the end of the last CAM cycle (Slave Relative).
- Profile switching can be done on the fly, without losing synchronization and without dead time.
- In addition, the offsets and ratios of CAM Profiles can be changed on the fly.
- See CAM Profile Switching for more information.
-
-
CAM objects are normally created in the Pipe Network using the graphical engine.
You do not have to add MLCamInit function blocks to their programs.
Parameters are entered directly in pop-up windows and the code is automatically added to the current project.
FBD Language Example
FFLD Language Example
IL Language Example
Not available.
ST Language Example
//Initialize a Pipe Network block named “CAM” with a profile named “Profile_A”, set the cam modulo position to 360
CAM := MLBlkCreate( 'CAM', 'CAM' );
MLCamInit( CAM, 'Profile_A', 360.0 );
See Also