MLPrfReadOScale
Function - Returns the Output Ratio value of a selected CAM Profile.
Inputs
|
Input |
Data Type |
Range |
Unit |
Default |
Description |
|---|---|---|---|---|---|
|
ProfileID |
DINT |
1 to 1024 |
N/A |
No default |
ID number of an initialized CAM Profile. |
Outputs
|
Output |
Data Type |
Range |
Unit |
Description |
|---|---|---|---|---|
|
Ratio |
LREAL |
|
|
Returns the Output Ratio value of a selected CAM Profile. |
Remarks
- Previous function name: MLPrfGetORatio
- Ratios can be changed on the fly to modify the CAM Profile while maintaining its basic shape.
- A change in output ratio is equivalent to stretching, and flipping if negative, the CAM Profile on the Y (or Output) Axis.
Figure 1: MLPrfReadOScale
FBD Language Example
FFLD Language Example
IL Language Example
Not available.
ST Language Example
//Save value of output ratio
CamRatio := MLPrfReadOScale( Profiles.Profile_A );
See Also