MLCompCheck

Pipe Network motion icon

 Function - Verifies if the reference of a comparator Pipe Block has been crossed.

Inputs

Input

Data Type

Range

Unit

Default

Description

BlockID

DINT

1 to 1024

N/A

No default

ID number of an initiated Comparator object.

Outputs

Output

Data Type

Range

Unit

Description

Default (.Q)

BOOL

FALSE, TRUE

N/A

Remarks

  • Returns the Transition Flag of a comparator object, which turns TRUE if the input position to the comparator is greater or equal to the reference.
    • The Comparator Transition Flag stays TRUE until it is reset.

Figure 1: MLCompCheck

FBD Language Example

FFLD Language Example

IL Language Example

Not available.

ST Language Example

//Check if Comparator Reference has been reached 
bCrossed := MLCompCheck( PipeNetwork.MyComp );

See Also