MLCompReadRef

Pipe Network motion icon

 Function - Returns the reference position of a comparator block.

Inputs

Input

Data Type

Range

Unit

Default

Description

BlockID

DINT

1 to 1024

N/A

No default

ID number of an initiated Comparator object.

Outputs

Output

Data Type

Range

Unit

Description

Reference

LREAL

 

 

Returns the current reference position of the Comparator object.

Remarks

  • The Transition Flag of a comparator object turns TRUE if the input position to the comparator is greater or equal to the reference.
  • The Comparator Transition Flag stays TRUE until it is reset.

FBD Language Example

FFLD Language Example

IL Language Example

Not available.

ST Language Example

//Return the Comparator Reference value
CompRef := MLCompReadRef( PipeNetwork.MyComp );

See Also