Convertor

Name

Description

MLCNVConECAT

Connects the output of a pipe convertor block to an EtherCAT Output (Rx) PDO object.

MLCNVConnect

Connects a converter Pipe Block to the specified axis.

MLCNVConnectEx

Connects the output of a pipe to an axis data other than the control position.

Connects an extra converter Pipe Block to the specified axis.

MLCNVDisconnect

Disconnect a converter Pipe Block from its associated axis.

MLCNVInit

Initializes a converter Pipe Block.

Purpose

Parameters

Associated Data

  • OutputValue: Output value of the data flows.
  • IslinkedToAxis: Boolean set to TRUE when the Convertor pipe block is linked to an axis block.