MLDerWriteInModPos

Pipe Network motion icon

 Function - Sets the Input ModuloPosition of the Derivator block.

Inputs

Input

Data Type

Range

Unit

Default

Description

ID

DINT

1 to 1024

N/A

No default

ID number of an initiated Derivator object.

ModuloPosition

LREAL

No range

User units

No default

Designated new value of Input ModuloPosition of the selected Derivator object.

Outputs

Output

Data Type

Range

Unit

Description

Default (.Q)

BOOL

FALSE, TRUE

N/A

Remarks

Input ModuloPosition is defined to manage the periodicity (modulo) of the input values.

Example

If the input value increases each millisecond by one degree then the output value is 1000 degrees per second.

Suddenly, the input value skips from 359 to 0 (zero).

  • Input ModuloPosition = 360, the output continues to indicate 1000 degrees per second.
    • This indicates that rollover into the next period has been properly handled
  • Input ModuloPosition = 1000, the output then indicates 359,000 degrees per second.
    • This indicates that the input has incorrectly interpreted roll-over as a 359 degree move in one millisecond.

Figure 1: MLDerWriteInModPos


  • The first calculation of a Derivator Pipe Block just after the pipe installation indicates 0 (zero) regardless of the initial input value.

FBD Language Example

FFLD Language Example

IL Language Example

Not available.

ST Language Example

//change the input MODULO_POSITION of a Derivator object to 720 
MLDerWriteInModPos ( PipeNetwork.MyDerivator, 720 );

See Also