MLTrigReadPos

Pipe Network motion icon

 Function - Returns the position of the block at the moment when it was triggered.

Inputs

Input

Data Type

Range

Unit

Default

Description

BlockID

DINT

1 to 1024

N/A

No default

ID number of an initiated Trigger object.

Outputs

Output

Data Type

Range

Unit

Description

Position

LREAL

No range

User units

Returns the position of the selected block's Axis at the moment when it was triggered.

Remarks

  • Returns the modulo-applied position of the pipe at the moment it is triggered by the Trigger Block's selected Fast Input.
  • This value is only valid when TrigIsTrigged() returns TRUE.
    • The Trigger block extrapolates the output value based on the timestamp of the Fast Input event to provide an accurate position even if the event occurs in the middle of a program cycle.
  • Once triggered, a block has to be reset before it can be triggered again.
    • All events sent to a block while in a triggered state are ignored.
    • The position and time information is lost.
  • Modulo Calculation: MLTrigReadPos uses the Output Modulo Position value of the previous block in the pipe, even if the previous pipe is configured for No Modulo mode.
    • The previous block must specify a 0 (zero) value for Output Modulo Position before setting the Mode to No Modulo to prevent a modulo operation for MLTrigReadPosPipe.
  • Previous Function Name: MLTrigGetPos

Fast Homing - Inputs

See these topics for more information:

FBD Language Example

FFLD Language Example

IL Language Example

Not available.

ST Language Example

//Save position of Axis when Fast Input event occurs
Trig_Position := MLTrigReadPos( PipeNetwork.TRIGGER );

See Also