FIFO

PLCopen motion icon

 Function Block - Manages a first in / first out list.

Inputs

Inputs

Data Type

Range

Unit

Default

Description

@Tail

ANY

 

 

 

  • Value of the oldest pushed value.
  • Updated after call.

Buf[]

ANY

 

 

 

Array for storing values.

IN

ANY

 

 

 

Value to be pushed.

POP

BOOL

 

 

 

Pop a new value on the rising edge.

PUSH

BOOL

 

 

 

Push a new value on the rising edge.

RST

BOOL

 

 

 

Reset the list.

Outputs

Outputs

Data Type

Range

Unit

Description

EMPTY

BOOL

 

 

TRUE if the list is empty.

OFLO

BOOL

 

 

TRUE if the overflow is on a PUSH command.

Count

DINT

 

 

Number of values in the list.

pRead

DINT

 

 

Index in the buffer of the oldest pushed value.

pWrite

DINT

 

 

Index in the buffer of the next push position.

Remarks

  • IN, @Tail, and Buf[] must have the same data type.
    • It cannot be a STRING.
  • The @Tail argument specifies a variable filled with the oldest push value after the block is called.
  • Values are stored in the Buf[] array.
    • Data is arranged as a roll over buffer and is never shifted or reset.
    • Only read and write pointers and pushed values are updated.
    • The maximum size of the list is the dimension of the array.
  • The first time an instance of the FIFO function block is called, that instance stores which array is passed to BUF[].
    • If a later call to the same instance passes a different array for the BUF[] argument, the call is considered invalid and no action is performed.
    • In this instance, the EMPTY output returns TRUE.

FBD Language Example

FFLD Language Example

  • In the FFLD Language, the input rung is the PUSH input.
    • The output rung is the EMPTY output.

IL Language Example

Not available.

ST Language Example

(* MyFIFO is a declared instance of FIFO function block: *)
MyFIFO (PUSH, POP, RST, IN, @Tail , BUFFER);
EMPTY := MyFIFO.EMPTY;
OFLO := MyFIFO.OFLO;
COUNT := MyFIFO.COUNT;
PREAD := MyFIFO.PREAD;
PWRITE := MyFIFO.PWRITE;

See Also

LIFO