derivate

PLCopen motion icon

 Function Block - Computes the derivative of a signal with respect to time.

Inputs

Input

Data Type

Range

Unit

Default

Description

RUN

BOOL

FALSE, TRUE

 

 

Run command:

  • TRUE=derivate.
  • FALSE=hold.

XIN

REAL

 

 

 

Input signal.

CYCLE

TIME

 

 

 

Sampling period.

Must not be less than the target cycle timing.

Outputs

Output

Data Type

Range

Unit

Description

XOUT

REAL

 

 

Output signal.

Remarks

  • The time unit is seconds.
  • The output signal has the units of the input signal divided by seconds.
  • The derivate block samples the input signal at a maximum rate of 1 millisecond.

FBD Language Example

FFLD Language Example

  • In the FFLD Language, the input rung is the RUN command.
    • The output rung keeps the state of the input rung.
    • ENO has the same state as RUN.

IL Language Example

Not available.

ST Language Example

(* MyDerv is a declared instance of DERIVATE function block. *)
MyDerv (RUN, XIN, CYCLE);
XOUT := MyDerv.XOUT;

See Also