GE >=

PLCopen motion icon

Operator - Tests if the first input is greater than or equal to the second input.

Inputs

Input

Data Type

Range

Unit

Default

Description

IN1

ANY_NUM

 

 

 

First input.

IN2

ANY_NUM

 

 

 

Second input.

Outputs

Output

Data Type

Range

Unit

Description

Q

BOOL

 

 

TRUE if IN1 >= IN2.

Remarks

  • Both inputs must have the same type.
  • Comparisons can be used with strings.
    • With strings, the lexical order is used for comparing the input strings.
      • Examples:
        ABC is less than ZX.
        ABCD is greater than ABC.

FBD Language Example

FFLD Language Example

  • In the FFLD Language, the input rung (EN) enables the operation.
    • The output rung is the result of the comparison.
  • The comparison is executed only if EN is TRUE.

IL Language Example

Not available.

ST Language Example

Q := IN1 >= IN2;

See Also