NE <>

PLCopen motion icon

Operator - Test if the first input is not equal to the second input.

Inputs

Input

Data Type

Range

Unit

Default

Description

IN1

ANY

 

 

 

First input.

IN2

ANY

 

 

 

Second input.

Outputs

Output

Data Type

Range

Unit

Description

Q

BOOL

 

 

TRUE if IN1 is not equal to IN2.

Remarks

  • Both inputs must have the same type.
  • Comparisons can be used with strings.
    • With strings, the lexical order is used for comparing the input strings.
      • Examples:
        ABC is less than ZX.
        ABCD is greater than ABC.
  • Equality comparisons cannot be used with TIME variables.
    • This is because the timer actually has the resolution of the target cycle and test can be unsafe as some values can never be reached.

FBD Language Example

NeFbd.gif (1232 octets)

FFLD Language Example

  • In the FFLD Language, the input rung (EN) enables the operation.
    • The output rung is the result of the comparison.
  • The comparison is executed only if EN is TRUE.

NeLd.gif (1441 octets)

IL Language Example

Not available.

ST Language Example

Q := IN1 <> IN2;

See Also