log / logL

PLCopen motion icon

 Function - Calculates the logarithm (base 10) of the input.

Inputs

Input

Data Type

Range

Unit

Default

Description

IN

REAL / LREAL

 

 

 

Real value.

Outputs

Output

Data Type

Range

Unit

Description

Q

REAL / LREAL

 

 

Result: Logarithm (base 10) of IN.

Remarks

None

FBD Language Example

FFLD Language Example

  • In the FFLD Language, the operation is executed only if the input rung (EN) is TRUE.
    • The output rung (ENO) keeps the same value as the input rung.
    • The function is executed only if EN is TRUE.
    • ENO has the same value as EN.

IL Language Example

Not available.

ST Language Example

Q := LOG (IN);

See Also