pow / powL

PLCopen motion icon

 Function - Calculates a power.

Inputs

Input

Data Type

Range

Unit

Default

Description

IN

REAL / LREAL

 

 

 

Real value.

EXP

REAL / LREAL

 

 

 

Exponent.

Outputs

Output

Data Type

Range

Unit

Description

Q

REAL / LREAL

 

 

Result: IN at the EXP power.

Remarks

None

FBD Language Example

FFLD Language Example

  • In the FFLD Language, the operation is executed only if the input rung (EN) is TRUE. 
    • The output rung (ENO) keeps the same value as the input rung.
    • The function is executed only if EN is TRUE.
    • ENO keeps the same value as EN.

IL Language Example

Not available.

ST Language Example

  • In the ST Language, the ** operator can be used.
Q := POW (IN, EXP);
Q := IN ** EXP;

See Also