ascii

PLCopen motion icon

 Function - Get the ASCII code of a character within a string.

Inputs

Input

Data Type

Range

Unit

Default

Description

IN

STRING

 

 

 

Input string.

POS

DINT

 

 

 

Position of the character within the string.

The first valid character position is 1.

Outputs

Output

Data Type

Range

Unit

Description

CODE

DINT

 

 

Either:

  • The ASCII code of the selected character.
  • 0 (zero) if the position is invalid.

Remarks

None

FBD Language Example

FFLD Language Example

  • In the FFLD Language, the input rung (EN) enables the operation.
    • The output rung (ENO) keeps the same value as the input rung.

IL Language Example

Not available.

ST Language Example

CODE := ASCII (IN, POS);

See Also

char