char
Function - Builds a single character string.
Inputs
|
Input |
Data Type |
Range |
Unit |
Default |
Description |
|---|---|---|---|---|---|
|
CODE |
DINT |
|
|
|
ASCII code of the specified character. |
Outputs
|
Output |
Data Type |
Range |
Unit |
Description |
|---|---|---|---|---|
|
Q |
STRING |
|
|
STRING containing only the specified character. |
Remarks
None
FBD Language Example
FFLD Language Example
- In the FFLD Language, the input rung (EN) enables the operation.
- The output rung (ENO) keeps the same value as the input rung.
IL Language Example
Not available.
ST Language Example
Q := CHAR (CODE);
See Also