PLS

PLCopen motion icon

 Function Block - Pulse signal generator.

Inputs

Input

Data Type

Range

Unit

Default

Description

RUN

BOOL

FALSE, TRUE

 

 

Enabling command.

CYCLE

TIME

 

 

 

Signal period.

Outputs

Output

Data Type

Range

Unit

Description

Q

BOOL

FALSE, TRUE

 

Output pulse signal.

Remarks

  • On every period, the output is set to TRUE during one cycle only.

Time Diagram

FBD Language Example

FFLD Language Example

  • In the FFLD Language, the input rung is the IN command.
    • The output rung is the Q output.

IL Language Example

Not available.

ST Language Example

(* MyPLS is a declared instance of PLS function block. *)
MyPLS (RUN, CYCLE);
Q := MyPLS.Q;

See Also