Tuning Controller Performance for EtherCAT Communication Latency
The response time for reading axis demand position data varies between different drive models.
- The response times also vary in reporting back TxPDO data such as actual position and time-based capture values.
- These different response times can lead to different lag in applications which use camming, gearing, and registration features.
- The KAS-IDE has several configuration parameters which allow you to tune your system to work best.
Example: Drive A has a 1 cycle latency for TxPDO data, and Drive B has 2 cycles latency.
The MC_AXIS_PARAM_VELCOMP_FACTOR parameter is used to specify 1 (for Drive A), and 2 (for Drive B) cycles.
The features and corresponding parameters are listed below.
-
- If the drives in an existing system are changed (e.g., during an upgrade from AKD to AKD2G drives), the parameters need to be retuned to maintain optimal performance.
|
Feature |
Parameters |
Read Me For More Information |
|---|---|---|
|
PLCopen Camming PLCopen Gearing |
Axis parameters:
|
|
|
PLCopen TouchProbe PLCopen Registration |
Axis parameter: MC_AXIS_PARAM_SENSOR_DELAY |
|
|
Pipe Network External Feedback |
Use a Phaser block to compensate for the delay |
|
|
Pipe Network Trigger Block |
Trigger Delay |
-
- The AKD drive supports an object to configure the EtherCAT input data for immediate or 1 cycle delay (default for backwards compatibility).