AXIS#.IL.CMD

Description

AXIS#.IL.CMD displays the q-component current command value of the current loop after any limitation (such as a parameter setting or I2t calculation).

AXIS#.IL.CMD is limited also by motor peak current, AXIS#.IL.LIMITN and AXIS#.IL.LIMITP.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read Only

Units

Arms

Range

± Drive peak current (IPEAK)

Default Value

N/A

(missing or bad snippet)

Float

See Also

AXIS#.IPEAK

Stored in Non-Volatile Memory

No

Variants Supported

All variants are supported

Related Topics

"Current Loop"

Industrial Ethernet Information

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

5801

1

5801 (0x16a9)

AXIS1.IL.CMD

Signed32

Read Only

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS1.IL.CMD

5801

Float

Read Only

-