AXIS#.MOTOR.IPEAK

Description

This parameter configures the drive for the motor's peak, instantaneous-rated current. AXIS#.MOTOR.IPEAK is used to limit the magnitude of the torque producing q-component current command (AXIS#.IL.CMD).


  • This parameter is required to be configured for all motor types.

Context

For more information see Motor.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

mA

Range

0.200 to 1,000

Default Value

2

Data Type

Float

See Also

AXIS#.IL.LIMITP, AXIS#.IL.LIMITN

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.MOTOR.IPEAK

500bh

12h

Unsigned32

-

1000:1

Read/Write

No

AXIS2.MOTOR.IPEAK

510bh

12h

Unsigned32

-

1000:1

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

6207

1

6207 (0x183f)

AXIS1.MOTOR.IPEAK

Unsigned32

Read Only

Yes

71743

2

6207 (0x183f)

AXIS2.MOTOR.IPEAK

Unsigned32

Read Only

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.MOTOR.IPEAK

6207

Float

Read Only

-